Skip to main content
Robot application
Triple arm
High res

Roboti in koboti za obločno varjenje FANUC

Roboti in koboti za obločno varjenje FANUC zagotavljajo vrhunsko natančnost in ponovljivost v panogi ter zagotavljajo brezhibne zvare pri vseh aplikacijah obločnega varjenja. Ponujamo obsežno paleto robotov in kobotov za obločno varjenje, ki podpirajo vse faze vašega delovanja, od brezhibne integracije za začetnike avtomatizacije do naprednih rešitev za izkušene uporabnike.

Prenesi za dodatne informacije

Dostop do bistvenih tehničnih specifikacij in dragocenih informacij o naših izdelkih prek naših dokumentov za prenos, ki vam bodo pomagali sprejeti prave odločitve in kar najbolje izkoristiti izdelke FANUC.

Navdihnite se

Navdihujte se pri uspehu drugih

Success story about the successful implementation of FANUC heavy-duty robot M-2000iA/2300 and a FANUC Arc welding robot at NTM's Finnish plant
NTM

Dvigovanje težkih tovorov za gradnjo tovornjakov

Družba NTM je lahko povečala proizvodno zmogljivost za svoja vozila za zbiranje odpadkov, saj se je odločila za avtomatizacijo nočne izmene. Z uporabo težkega robota, ki lahko dvigne do dve toni, in varilnega robota, lahko finska tovarna podjetja zdaj dela brez osebja ponoči ali ob koncih tedna.

Success story about successful implementation of FANUC welding robots at the Italian company Bonvicini Carpenteria S.r.l.. Bonvicini S.r.l, a contract welding specialist, has invested in new industrial robot technology to meet customer demands for increased flexibility. In addition to their long-standing use of FANUC robots and with the help of system integrator company TECNOROBOT they have introduced their first collaborative robot, a FANUC CRX-10iA/L, which was up and running in 1 hour.
Bonvicini Carpenteria S.r.l.

FANUC's CRX Cobot Boosts Production Flexibility

Bonvicini Carpenteria today enjoys even higher levels of quality and flexibility. The company can flex between automation solutions whenever production volumes dictate. In particular, Bonvicini Carpenteria is taking advantage of easy and fast robot programming with features such as drag and drop functionality and a simple tablet interface.

FANUC R-2000iC industrial robot and Arc Mate 100iD arc welding robot boosting the production of car seat structures at Brose Sitech.
Sitech

FANUC Robots Put Brose Sitech in the Driver’s Seat

The automotive industry is notorious for its high productivity demands, narrow profit margins and rigorous quality standards. Automation is essential to ensure reliable, repeatable, cost-effective production with maximum uptime. The choice of robot supplier, therefore, is nothing less than critical.