Skip to main content
The FANUC SR-3iA robot picking peanuts.

Serija SCARA

Povečajte hitrost in natančnost z robotom FANUC SCARA. Iščete način za povečanje hitrosti, natančnosti in ponovljivosti v proizvodnih procesih, ki zahtevajo obremenitve do 20 kg? Naša linija robotov SCARA se uporablja v vseh vrstah aplikacij za rokovanje.

Prenesi za dodatne informacije

Dostop do bistvenih tehničnih specifikacij in dragocenih informacij o naših izdelkih prek naših dokumentov za prenos, ki vam bodo pomagali sprejeti prave odločitve in kar najbolje izkoristiti izdelke FANUC.

Navdihnite se

Navdihujte se pri uspehu drugih

Success Story AlphaRobotica pictures and media
Alpha Robotica

Roboti FANUC pomagajo proizvajalcu mask pri spopadanju z izzivi

Kadar se povpraševanje po proizvodnji v kratkem času močno poveča, lahko roboti in avtomatizacija pomagajo izpolniti zahteve veliko hitreje, kot se mnogi zavedajo. Vendar je ta rezultat močno odvisen od izbire robotov, ki jih je enostavno namestiti, programirati in zagnati.

Success story about automated placing into packaging trays using FANUC robots by the Swiss company Kunststoff-Packungen AG. 

FANUC enabled Kunststoff-Packungen AG to run the manufacturing line autonomously, with autonomous operation for at least 8 hours at full speed, achieving cycle times of 0.8 seconds. The project involved two FANUC robots: a six-axes M-10iD/10L with a payload of 10 kg, and a four-axes SR-6iA robot with a 6 kg payload. Significant space saving was achieved because of the compact footprint of the solution.
Kunstoff-Packungen AG

Placing Plastic Injection-Moulding into Packing Trays

Because manufacturers everywhere face shortages of skilled labor, and as a company dedicated to excellence, Kunstoff-Packungen continuously seeks ways to improve its level of automation.

FANUC enabled Vernay to fully automate, in a single cell, a production process involving flow-control solutions, and can now produce parts 24 hours and 7 days without interruptions.
A SCARA robot, the FANUC SR-6iA, is used for picking, placing, and quality control, and the FANUC FANUC M-20iD is employed to flexibly load and unload a moulding machine.
Vernay

Loading & Unloading, Flex Feeding, and Inspection in a Single Cell

Vernay is globally renowned for flow control solutions, producing over a billion rubber valve components annually across Asia, the Americas, and Europe. Their critical products, used in devices like respirators and EV battery systems, must meet the highest quality standards with zero defects.