Akim Metal - SMB

CNC Lathe Builder Takes Control of Production with FANUC

In a world of increasingly complex engineering components, machine tools require ever-more capabilities and functions. The humble lathe, a mainstay of the machining industry, is a case in point. The SMB brand of Türkiye-based Akim Metal today builds lathes with servo-controlled twin turrets, programmable steady rests, live tools, programmable tailstock and integrated automation. To provide optimal process control in the hunt for ever higher component quality, repeatability and productivity, the company takes advantage of FANUC CNC systems.
How to produce Advanced Technology

Key Insights from Task to Result

Task

Modern users of SMB CNC lathes require far more than conventional capabilities such as face and outside diameter turning. For today’s performance-hungry machine shops, the more operations the lathe can complete in a single set-up, the better. SMB offers core products such as its flagship TT850 and TT550 series twin-turret lathes to meet this demand. However, precise process control is vital. 

Solution:

FANUC’s 0𝑖-TF Plus provides the answer. This fundamental CNC system is tailored to turning applications, optimally enhancing lathe functionality. Akim Metal SMB also takes advantage of the quality and reliability of FANUC motor technology, as well as FANUC’s automation solutions and extensive knowledge.

Result

With FANUC technology, SMB lathe customers are able to perform additional operations such as bevel turning, hole drilling, chamfering, grooving, profile turning, threading, tapping and die drawing - in a fast, reliable, highly repeatable and precise manner. Eccentric parts also prove no problem thanks to the dual-path feature offered by the FANUC control, which manages the two turrets independently. Put simply, users of SMB twin-turret lathe users are able to complete more work in less time.

About Akim Metal

Akim Metal - SMB Case Study picture
Thanks to FANUC’s 0i-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations in a rapid, highly repeatable and accurate manner

Akim Metal SMB can call upon more than 50 years of experience as a manufacturer of lathes for sectors that include automotive, white goods, industrial motor and aerospace. Based in Istanbul, the company produces CNC lathes with integrated automation systems to provide its customers with high-technology solutions. Its three principles of quality, cost and delivery underpin a customer-oriented approach. Akim Metal SMB carries ISO 9001, ISO/TS 16949 and ISO 14001 accreditations.

FIND OUT MORE ABOUT AKIM METAL

FANUC CNC Provides Optimal Enhancement of Lathe Functionality

Akim Metal SMB uses its knowledge and experience to offer customers high-technology CNC lathes featuring integrated automation. A good example is its twin-turret TT850C and TT550C series, which feature a powerful spindle, programmable steady rest, servo-controlled turrets, programmable tailstock and optional live tools. To control these advanced machines, the company relies on FANUC CNC systems.

“Our R&D team works in close liaison with FANUC to ensure our customers can take full advantage of the stable and reliable control infrastructure offered by FANUC,” reveals Ali Fazil Böyet, General Manager at Akim Metal. 

Thanks to solutions such as FANUC’s 0𝑖-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations such as face turning, OD turning, bevel turning, hole drilling, chamfering, grooving, profile turning, threading, tapping and die drawing in a rapid, highly repeatable and accurate manner.

Akim Metal - SMB Case Study picture
Thanks to FANUC’s 0i-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations in a rapid, highly repeatable and accurate manner
Akim Metal - SMB Case Study picture
Thanks to FANUC’s 0i-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations in a rapid, highly repeatable and accurate manner
Testimonials quote

Ali Fazil Böyet

General Manager

With the dual-path feature offered by the FANUC 0𝑖-TF Plus, users gain the ability to manage two turrets independently. This function provides superior efficiency in multi-axis and complex machining processes, as well as fast cycle times. Ultimately, users can complete more orders in less time. 

But CNC systems are only part of the offer provided to Akim Metal SMB. With FANUC’s automation solutions, the machine tool builder can ensure its customers benefit from seamless robot integration, tool-changing systems and automatic loading/unloading, while contributing to in-plant digitalisation processes through communication protocols compatible with Industry 4.0. 

Akim Metal - SMB Case Study picture
Thanks to FANUC’s 0i-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations in a rapid, highly repeatable and accurate manner

“Thanks to our strong collaboration with FANUC, we integrate the latest automation and CNC technologies into our production processes and continue to manufacture high-performance, reliable machines,” he states. “At the same time, our close work with the FANUC service and engineering team in Türkiye allows our efficient production processes to continue uninterrupted.” 

Akim Metal SMB says it is carrying the company’s production into the future with FANUC technologies and making a difference in the industry with automation-enabled and digital transformation-oriented machine tools. 

Akim Metal - SMB Case Study picture
Thanks to FANUC’s 0i-TF Plus CNC and superior motor technology, SMB lathe users are able to perform operations in a rapid, highly repeatable and accurate manner

“We believe our co-operation with FANUC - which combines high precision, quality and efficiency - will continue to make significant contributions to future production technologies,” concludes Ali Fazil Böyet.

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.