14 places means that the robots have long paths. Therefore, both FANUC robots have been assembled on a 13 metre long linear axis. The robots have a load capacity of 45 kg and a maximum reach of 2,606 mm. In principle, the task is divided easily between the two robots M-710iC/45M: Robot 1 approaches spaces 1 to 7, robot 2 approaches spaces 8 to 14. So long as the robots do not travel beyond their respective borders, it is enough to protect them using “Dual Check Safety” (DCS). Another safety option from FANUC, Interference Check, prevents the robots from colliding with one another in dynamic operation. Bürgermeister sees both options as useful: “Either we block the areas or we make a dynamic request. Both are technically feasible.”