Skip to main content
Media data stream portal

News & Media

The latest news, case studies, as well as upcoming events from the world's leading supplier of factory automation.

Case Studies

Discover remarkable accomplishments fueled by FANUC's factory automation solutions. See how our technology transforms industries and propels success.

Images case study Phytopharm Klęka S.A from FPL. CRX-20iA/L handles bottle stacks using a custom vacuum gripper, while a CRX-25iA palletises heavy product cartons.
Phytopharm Klęka S.A.

From Pallet to Product: FANUC Cobots enhance Pharma Packaging

Phytopharm Klęka S.A., a market leader in plant-based products for pharmaceuticals and cosmetics, has improved packaging ergonomics, flexibility and reliability through the adoption of two collaborative robots (cobots) from FANUC. By automating bottle de-palletising and carton stacking in collaboration with ZW Automation, the company is exceeding initial performance estimates of cobots while improving safety and reducing worker monotony. Supported by FANUC palletising software and intuitive operation, the cobots deliver a more agile and efficient three-shift manufacturing environment.

Images Swissmint case study
Automated milling cell with FANUC ROBODRILLs and M-20iD/25 robots
Images Radmot case study
Automated milling cell with FANUC ROBODRILLs and M-20iD/25 robots
RADMOT

FANUC robots enable 24/7 CNC machining at RADMOT

Automated CNC machining cells comprising various machine tools and robots require astute design and integration. So why not simplify the process by turning to the world’s most prominent manufacturer of both CNC machine tools and robots: FANUC. That was precisely the strategy of RADMOT, a major Poland-based provider of machining services when it wanted to implement a new CNC milling cell involving three machining centres and two robots that could run unmanned 24 hours a day, 7 days a week – without any collisions between robots.

Images WU GmbH Case study featuring and LR-10iA/10 and ROBODRILL.
WU Mechanische Werkstätte GmbH

Success of FANUC Robot Cell Leads to New Revenue Stream

What do most contract machining companies consider when looking to reach the next level of efficiency, productivity and reliability? The answer, of course, is automation. For this very reason, Germany-based WU Mechanische Werkstätte GmbH built an automation cell -featuring a FANUC industrial robot - for loading and unloading one of its own machine tools. Two years later, a visitor liked the concept so much he asked WU to build him one. This marked the beginning of an additional revenue stream based on the design and build of automation cells featuring high-performance industrial robots from FANUC.

Images Eugster/Frismag Case Study. Assembling of coffee grinders with LR Mate 200iD/7L and handling with M-20iD/25 in combination with ZDT.
Eugster/Frismag

Fully Automated Assembly of Coffee Grinders

In the manufacture of popular household appliances such as coffee grinders, a number of prerequisites determine production success. For instance, only clearly structured, efficient and target-orientated processes will result in the required levels of production reliability. Achieving this ambition becomes significantly more realistic using automation, as market leader Eugster/Frismag AG can testify following its adoption of 14 FANUC LR Mate industrial robots and FANUC ZDT (Zero Down Time), which now enable the continuous automated assembly of a coffee grinder every 7 seconds.

Images Inoverde Case Study. Picking, Packing, Palletising of carrots with M-20iD/25, M-20iD/35, and M-710iC/50 and DCS.
Inoverde

Trio of FANUC Robots Boost Packing Efficiency at Inoverde

In a fast-moving fresh-food distribution plant, efficiency through automated packing operations is paramount to keep pace with demand. As a by-product of this approach, robot adopters also gain from less physical strain for employees, gentler handling of delicate produce like fruit and vegetables, and more a uniform and repeatable process. Among the latest factories to benefit from all this added value is the Bätterkinden, Switzerland facility of major food distributor Inoverde, where carrot filling, packing and palletising operations are benefiting from the introduction of three FANUC industrial robots.

Images FFG Werke case study: Pick-up vertical turning machines for top production quality featuring CNC Series 31iB Plus
FFG Werke

Multi-capability FANUC CNC takes Vertical Turning to New Heights

Developing a new take on an age-old process such as turning requires superhuman levels of creativity and innovation. Moreover, converting those new machine visions and concepts into reality necessitates extremely advanced control technology. With this thought in mind, machine tool builder FFG Werke knew exactly where to turn for a CNC system with necessary capability and performance to complement its groundbreaking new vertical turning centre: FANUC.