Biblioteca y compilador de MACROS



La función Macro Executor, su potente lenguaje de programación para la gestión de máquinas o mecanizados, convierte, carga y ejecuta programas de macros personalizados (macro de P-CODE) en F-ROM (memoria flash de CNC). Entre las ventajas de este lenguaje, se incluyen la ejecución de códigos a gran velocidad, la máxima protección de programas, los procedimientos de llamada sencillos y la ampliación del conjunto de funciones de control CNC.

Benefits

  • Creation of customized functions and programs
  • Modification of Macro Programs to follow machine and production evolution
  • Powerful programming language for machining or machine management purpose

Some NC programs such as technology functions or programs created using custom macros do not need to be modified once created. Other NC programs, such as machining programs, evolve during machining.

The Macro Executor function can convert a Custom Macro program created by the machine tool builder to an executable macro program, load the executable macro programm (P-CODE macro) into F-ROM (CNC Flash Memory), and execute it.

The function which converts a Custom Macro program to an Executable Macro program is called the Macro Compiler. The function which reads and executes a P-CODE macro is called the Macro Executor.

The Macro Library is part of the CNC Application Development Kit.