Albiez: “We develop the systems during discussions. It’s normally a process.“ Wagner knows what he’s letting himself in for: “Without Robotec Engineering as our systems partner, we wouldn’t be able to do it.” The facility was developed with the support of Roth Technik, Sulgen. The owner, Markus Roth: “We offer all sub-disciplines of automation and also build turnkey solutions. The small mechanical engineering company has distinguished itself, above all, with the development of the gripper. “We start with standard components that we adapt to the specific task and then develop it further. For example, by integrating a camera, as in the case of Rau.”
Low-machining materials are a main focus. In general, however, Herbert Wagner takes a close look at whether a new component fits into his “formula”. And what makes Rau so special? Wagner: “If you want a good service at a fair price, then we’re the partner for you. We are a complete service provider for parts and components and are able to use our experience to also support customers in the development of parts.”
Instead, a camera provides the solution. As the gripping positions and the required conveying devices are located between the machines, the camera could have been placed very high up, underneath the robot's track. Alternatively, it would have been necessary to install a camera on each side. The first option, however, would not have provided satisfactory results and the second option would be too costly with the need for the additional camera. Because the gripper also reaches into the machine with all the chips and cooling lubricant, the camera would have quickly become “blinded”. As a result, the camera was installed in the gripper, but in a box that is opened by a pneumatic cylinder. Adrian Albiez says of the advantages of this solution: “The camera can be set for an optimum range, it is not in the way and it is always protected.” And Robotec Engineering: provided yet another constructive experience here: all the cables and hoses are guided inside the gripper. “This prevents premature wear of the energy and media lines.”