FANUC Empowers Europe’s Machine Tool Industry in Times of Change
The European machine tool industry is facing numerous challenges: a shortage of skilled workers, rising cost pressures, and geopolitical shifts. Traditional customer groups such as automotive manufacturers and suppliers are undergoing restructuring and reducing their investments, while other export-oriented sectors are postponing investments due to tariff disputes and potential trade restrictions. In this challenging environment, FANUC, as a global leader in factory automation solutions, supports the machine tool industry with innovative technologies and long-term service. A key focus is on making products easier to operate and gradually evolving existing systems.
“Our latest FANUC CNC Design Studio is an integrated development environment which consolidates the data for CNC settings, offers efficient debugging functions and facilitates the conversion towards our latest CNC generation 500𝑖-A,” explains Robert Koopmann, Chief Technology Officer at FANUC Europe.
Advanced AI-driven features, including FANUC’s Smart Digital Twin, help machine tool builders and end-users optimise performance, e.g. by reducing cycle time and improving surface quality. Automation with FANUC robots also enables the existing workers to focus on higher-value tasks. Connecting a FANUC robot to a FANUC CNC-controlled machine tool has been further simplified and now requires only minimal configuration effort Energy efficiency and cost competitiveness are also top priorities in the factory automation business: FANUC’s latest servo drive series, the αi-D, delivers a 10% to 15% reduction in power loss and up to 30% space savings compared to previous models, while boosting speed and precision. Standardised solutions further accelerate automation deployment.
As companies increasingly evaluate the total cost of ownership (TCO) of their equipment, FANUC is reinforcing its commitment to life-long product support. The new FANUC Care program offers peace of mind by covering all non-customer-caused repairs for up to eight years after purchase.
With over 280 locations and multiple warehouses worldwide, FANUC ensures fast delivery and responsive customer service. This global presence is becoming increasingly relevant at a time when manufacturers are reassessing the geographic distribution of their production networks. FANUC’s IoT solutions enable remote monitoring and maintenance; capabilities that proved essential during border closures and supply chain disruptions. Cybersecurity is another focus on FANUC’s development: “As production becomes more global and interconnected, cybersecurity is paramount,” emphasises Koopmann.
FANUC’s latest CNC generation, the 500𝑖-A, and the R-50𝑖A robot controller meet the highest cybersecurity standards. The IoT platform FIELD system Basic Package has also been designed with robust cybersecurity features at its core. "With 70 years of experience in factory automation and fully automated in-house production facilities, FANUC understands the challenges facing the machine tool industry," says Koopmann. "Our development teams are committed to helping our customers prepare for the future."