Skip to main content
PHYSICAL AI 
WEBSITE ONLY

Physical AI for Industrial Robotics and Automation

Discover how open platforms and Physical AI can transform your automation strategy, giving you the flexibility to scale, adapt, and integrate advanced capabilities that elevate performance across your entire production environment.

Physical AI Applications

Physical AI enables robots to perceive, adapt, and act in real-world manufacturing environments. These applications highlight how FANUC robots can use AI, real-time control, natural language instructions, and simulation to perform complex automation tasks with greater flexibility and precision.

AI Robot Tracks Moving Parts and Tightens Screws

FANUC robots can identify and track workpieces moving in three dimensions, following them precisely in real time. This enables operations such as tightening screws on moving parts, a task that traditionally required precise fixturing or part stabilisation. With 1 millisecond high‑speed tracking performance, high-speed 3D tracking ensures consistent accuracy even in dynamic environments.

Explore Inbolt AI Vision Guidance
Image for AI webpages. Website only. Dynamic line tracking Inbolt.
Image for AI webpages. Website only.

AI Agent-Driven Kitting Operations

By issuing instructions in natural language to the AI agent for tasks like photographing order forms, recognising text, and transporting trays and parts, a robot can execute the kitting of workpieces. By combining an AI agent, which understands natural language to control the robot and autonomously execute tasks, with a masterless AI recognition function that identifies objects based on natural language inputs, it becomes possible to modify operation logic, just as if instructing a human.

AI Robot with Dynamic Proximity Monitoring

FANUC robots equipped with AI-driven perception can detect nearby people and adjust their paths in real time without stopping production. Using the torque command input of the “Stream Motion” function, the force generated by the robot arm is limited within a safe operating range. If a human enters the robot’s working area, the robot automatically modifies its trajectory to avoid contact. Once the area is clear, the robot returns to its original path and continues the task. This enables safe, uninterrupted collaboration on the factory floor.

Image for AI webpages. Website only.
Image for AI webpages. Website only.

AI Controls Dual Arms to Install a Flexible Cable

Using Vision-Language-Action (VLA) foundation model, two FANUC robot arms can work together to imitate human tasks, like folding a t-shirt or performing highly dexterous wiring operations. The system detects cable tension in real time and manipulates soft, flexible cables with human-like sensitivity. Leveraging multi-axis articulation, the robots route cables across complex 3D paths, including height, depth, and tilt, while maintaining accurate handling and preventing damage.

Robot Programming by Voice with Generative AI

FANUC robots can recognise voice commands in multiple languages, automatically generate Python programs using generative AI, and execute the resulting tasks while perceiving their surroundings. Users provide instructions verbally, and the robot interprets the language, generates the appropriate program and carries out the requested action.

These capabilities also support complex tasks such as:

Rolling a die and placing it in the correct location based on the number shownStacking a die of a specific color on top of another

These tasks previously required specialised programming but can now be executed through intuitive voice commands.

Image for AI webpages. Website only.
Image for AI webpages. Website only.

Advanced Simulation and Digital‑Twin Support

FANUC supports advanced simulation and digital‑twin technologies that allow manufacturers to design, test, and validate robotic systems before deployment. Photorealistic virtual factory environments help teams model robot behavior, evaluate cell layouts, and optimise performance in a risk‑free setting. By using NVIDIA Isaac GR00T to train the robot motion and object behavior, the robots autonomously learn to handle previously “unseen” situations. FANUC robots are available in formats suitable for modern simulation platforms, enabling cycle‑time analysis, trajectory validation, and AI training data generation in virtual production workflows. These tools shorten commissioning time and improve overall system accuracy.

Enhanced Integration with FANUC Simulation Tools

FANUC’s simulation ecosystem—such as its offline programming tools—supports the exchange of trajectory and performance data with external simulation environments. This allows developers to model real robot behavior with greater fidelity and validate system performance earlier in the design process.

Image for AI webpages. Website only.

Physical AI: Frequently Asked Questions

Physical AI is reshaping industrial automation by combining robotics, artificial intelligence, real-time control, simulation, and open development platforms. Explore answers to common questions about how FANUC supports Physical AI, how these technologies work together, and how manufacturers can use them to build more flexible, intelligent, and adaptive automation systems.

Frequently Asked Questions

Physical AI refers to artificial intelligence that can perceive the real world, make decisions, and take physical action through machines such as industrial robots. In manufacturing, Physical AI enables robots to understand their environment, adapt to changing conditions, and perform complex tasks with greater autonomy.

FANUC supports Physical AI through open platform technologies such as ROS 2 support, Python programming, real-time motion control with Stream Motion, digital-twin simulation capabilities, and collaborations with global technology leaders. These tools help developers and manufacturers build intelligent automation systems that can perceive, adapt, and act.

ROS 2 is important because it provides a flexible framework for connecting robots, sensors, motion planning tools, simulation platforms, and AI applications. FANUC’s ROS 2 driver helps developers integrate FANUC robots into modern robotics workflows, including MoveIt, simulation, and advanced robot control.

Developers can get started by exploring the FANUC ROS 2 driver, robot description packages, Stream Motion capabilities, Python programming support, and FANUC’s simulation tools. These resources help teams connect FANUC robots with modern AI, robotics, and automation development environments.

Traditional industrial automation often relies on fixed programming, structured environments, and repeatable tasks. Physical AI adds perception, learning, simulation, real-time control, and adaptive decision-making, allowing robots to respond more intelligently to dynamic production environments.

FANUC is working with technology leaders such as NVIDIA and Google to advance Physical AI through areas such as digital twins, real-time simulation, imitation learning, generative AI, AI-powered robot programming, and advanced robotics software. These collaborations help make industrial robots more intelligent, adaptable, and easier to use.

Yes. FANUC robot controllers can execute Python programs directly, allowing users to apply AI models and automation logic developed in Python. This helps bridge the gap between AI development and industrial robot control.

Real-time motion control allows a robot’s position, speed, and torque to be adjusted with extremely fast communication. FANUC’s Stream Motion capability supports high-speed control, enabling applications such as trajectory tracking, adaptive movement, and AI-guided automation.

*ROS is a trademark of the Open Source Robotics Foundation. 

**Python is a registered trademark of the Python Software Foundation. 

***GitHub is a registered trademark of GitHub, Inc.