Skip to main content
Etasis

Break Up Long Chips with FANUC Servo Learning Oscillation Function

Long chips from machining operations disrupt machine function. ETASIS, a Turkish tool producer, sought a solution. FANUC’s CNC offers the Servo Learning Oscillation Function, which oscillates the tool along the cutting direction, maintaining quality and reducing cleanup. This solution is essential for robotic machine tending and eliminates the need for chip-breaking equipment. ETASIS is highly satisfied with the results.
ETASIS is offering their customer the perfect solution by using FANUC’s CNC and specifically the Servo Learning Oscillation Function, which eliminates the need for chip breaker equipment resulting in significant labour savings and enhanced quality.

Key Insights from Task to Result

Task

For many machining operations, long chips are a problem. The stripes of coiled metal can wrap around the workpiece and the cutting tool and interfere with the proper operation of the machine tool. ETASIS, a Turkish producer of custom machine tools, wants to provide their customers with a solution that eliminates the long chip problem. These curly chips are especially problematic when lathing, but also can occur with other operations such as drilling and milling.

Solution

FANUC’s CNC provides a software application called the Servo Learning Oscillation Function. This function causes the tool to oscillate along the cutting direction. By applying Servo Learning Control, the oscillation is accomplished without compromising quality or accuracy.

Result

The Servo Learning Oscillation function enhances the quality of the finished product. Significant labour savings are achieved by avoiding the need to clean off parts. For those customers who wish to use a robotic arm for machine tending, eliminating the long chip problem is crucial. FANUC’s software solution eliminates the need for chip-breaking equipment. ETASIS is very pleased with the results of this function.

Etasis

ETASIS has been producing CNC machines since 1990, and they are proud of their team’s ability to adapt to new technologies. All of their products are of their own design, and they make special machine tools for a variety of industrial sectors.

FIND OUT MORE ABOUT Etasis
Thanks to FANUC’s CNC and specifically the Servo Learning Oscillation Function, the Turkish company ETASIS, eliminates the need for chip breaker equipment resulting in significant labour savings and enhanced quality.

FANUC CNC Machines Help Shape the Future at Moulding Specialist

ETASIS produces custom machine tools for many applications, including high-technology end-users like automotive and aerospace. Long, coiled chips can cause many problems such as conveyor stoppages, substandard surface finishes, and reduced tool life.

Meliha Günaltin, General Manager at ETASIS, explains: "The FANUC Servo Learning Oscillation function increases the production quality of the machines we produce. In materials and processes with a high probability of chip wrapping, the chip formed cannot be removed and causes quality loss with time when the part is processed with traditional methods."

"In mass production areas, the chip formed needs to be cleaned off the part, for continuing the next processes smoothly. This causes additional labour requirement and costs. In addition, a chip-free workpiece is inevitable for customers who want to implement a robotic automation system such as machine loading and unloading. In various tests with the FANUC Servo Learning Oscillation application, we eliminated the chip off the part."

ETASIS testimonial Image related to the ETASIS success story.
Testimonials quote

Meliha Günaltin

General Manager

Ms. Günaltin goes on to explain how they utilise the function:

"After the suitable cutting conditions of the workpiece are determined, the specified conditions are entered into the setting instructions of the Servo Learning Oscillation application and the function is ensured to run smoothly. We carried out R&D studies to determine the optimum values for the chip-breaking function.

We also use it for drilling and milling machines along with lathes. The FANUC Servo Learning Oscillation application eliminates the need for chip breaker equipment and for additional labor. It provides us with high benefits in terms of cost and time. In addition, this function extends the tool life, providing a significant cost reduction and efficiency in production."

FANUC CNC Servo Learning Oscillation function lets your tool oscillate along the cutting direction to break chips effectively and efficiently in turning and drilling operations - without compromising accuracy. The oscillating tool produces small chips, avoiding the entanglement of large, twisted chips

Get Inspired

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.