New ROBODRILL series

The new FANUC ROBODRILL series is advancing

PRESS RELEASE

September 5th, 2016

Echternach - We are proud to announce the new generation of ROBODRILL machines, which we will present at the AMB Show in Stuttgart from 13 to 17 September (stand B51 in hall 7).

The new α-DiB series will take over from our successful α-DiA series. It comes with a variety of improvements and new features. The biggest change is the introduction of advanced machines.

With the new series, we offer both standard and advanced models in the known sizes (S, M, L). So there are six ROBODRILL machines to meet the needs of our customers. 

Both the standard and advanced models have an operator`s panel equipped with our new iHMI to make them easy to use. The Operation Management Software ‘ROBODRILL-Linki’ permanently monitors the machine, providing operation results as they occur. Automatic machine monitoring keeps downtimes to a minimum.

In line with our philosophy, the new ROBODRILL can be easily automated with FANUC Robots. Our ‘Quick & Simple Start-up Package’ simplifies the automation of the ROBODRILL with a FANUC Robot, saving you time and money.

We have reduced cycle time by using new smart functions for rapid traverse and tool changing. Also, the new machines have been designed to make maintenance even quicker and as easy as possible, thanks to an improved Preventive Maintenance Guidance feature.

From 2017, all models can be equipped with the new DDRiB rotary table or DDR-TiB trunnion system with an indexing time of 0.55 seconds – a reduction of 0.3 seconds – and very fast clamping. The clamping torque has been increased to 700N-m.

Our advanced α-DiB models offer the following extra technical improvements.

  • Z-axis strokes reach 400mm to produce larger parts, reducing the interference among tools and the workpiece.
  • An extra servo motor has been installed in the turret to reduce the tool-change time to
    0.7 seconds – 0.2 seconds faster than the standard version – for faster cycle times and increased productivity.
  • Advanced models now accept larger tools of up to 4kg.

Standard models from the α-DiB series will be available for European customers from the autumn of 2016. Advanced models will be available in early 2017.