As efficient as a new one after 35 years
This is why the responsible persons went on a quest to find a new, suitable jig grinding machine – and rather by chance happened upon Roland Haslebacher. He promised them that he would lift the Hauser S3 to a modern CNC level. For good measure, he had the X/Y table laser-measured. The result of the ISO measurement was a non-conformance of merely 0.0025 mm – “a great value for a 35-year-old machine,” specialist Roland Haslebacher assesses. “The only change to the mechanics was the replacement of the frontal spindle bearings. Other than that, the entire electrical installation including CNC came up for renewal.”