Sustainability
Stock Image

Water Resources

With a focus on sustainability, FANUC diligently manages water resources to protect the environment and promote a greener, more sustainable world.

Reusing Water

Collaboration with Suppliers

Because water resources are used by our suppliers in the process of cooling castings and by our customers in the process of using our products and systems, indirect use of water resources is also an important issue. FANUC, therefore, are asking suppliers to adopt our CSR Procurement Policy, and to promote the efficient use and cyclical use of water resources. 

A total of twelve companies, namely two manufacturing subsidiaries and ten suppliers whose sales to FANUC account for more than 30% of their total sales, are surveyed once a year on specific matters such as water consumption and water emissions. The results are then quantified for evaluation, based on which risks are identified and assessed. We select the top three companies that are defined as significant, set specific goals for reducing the environmental load of their production, and encourage them to take steps toward those goals. In the event of significant changes in the numbers, we check the reasons for those changes and provide advice, as necessary.