FANUC exhibiting at the Interpack 2017

Visit the FANUC booth at the largest packaging fair from May 4 – 10 in Düsseldorf, Germany

Echternach, Luxembourg – FANUC will attend the largest, worldwide trade show – Interpack - for the packaging industry in Düsseldorf, Germany.

At this year’s Interpack, FANUC will exhibit a diverse range of robots, simulation software and a multi-axis automation solution, which will enable customers to build their own pick and place, sorting, packaging and palletising solutions. The FANUC booth will be located in Hall 6, Booth D79.
Besides experiencing FANUC products live, it allows visitors to directly communicate with experts. They will receive first-hand information about the various features and functionalities of the products on display.

At FANUC’s booth, visitors will have the chance to see several robots in action. The M-410iC/500 will be demonstrating how it easily handles a heavy payload (500 kg). In the meantime, the M-2iA robot model picks and places bottles. The palletising robot M710iC/50H showcases its ability to work in highly compact spaces thanks to its slim wrist. Both robots will demonstrate their high speed while performing these task. The latest Cleanroom robot addition, the M-20iB/25C with IP 67 standard, will also be present on the booth. This special white coat model is highly suitable for cleanroom environments such as 2nd-Food areas or the medial, optical, pharmaceutical or electronics industry.

FANUC’s robot simulation software – ROBOGUIDE – will be available for testing to visitors. In self-designed robot cells, they can explore the possibilities of simulating robot motions, and application commands to achieve high cost-efficient designs before purchasing a robot.

Visit the FANUC booth in Hall 6, booth D79 from May 4 – 10 in Düsseldorf, Germany!



About FANUC

FANUC Corporation is the worldwide leading manufacturer in factory automation for CNC control systems, robots and production machinery (ROBODRILL, ROBOCUT and ROBOSHOT). Since 1956, FANUC has been a pioneer in the development of computer numerical control equipment in the automation industry. With more than 252 offices worldwide and more than 6.500 employees, FANUC offers a vast network for sales, technical support, logistics and customer service.

Legend:

PR Contact:

More information can be acquired here:
FANUC Europe Corporation S.A.
7, rue Benedikt Zender
L-6468 Echternach

Phone : +352 (0)72 7777-0
Email : pr@fanuc.eu
Home: www.fanuc.eu

Nigel Ramsden Manager European Technical Support RO, Technical Sales Support RO
7, rue Benedikt Zender
L-8467 Echternach

Tel.: +352 (0) 72 7777 450